REC.TRIGSLOPE

Description

REC.TRIGSLOPE sets the recorder trigger slope. This parameter is not used when REC.TRIGTYPE is 0 or 1.

Value Description
0 Negative
1 Positive

Example

Code

Trigger the capture on a positive rate of change.

-->REC.TRIGSLOPE 1

Context

For more information see Scope.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

1

Data Type

Integer

See Also

REC.TRIG, REC.NUMPOINTS

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

2309

1

2309 (0x905)

REC.TRIGSLOPE

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

REC.TRIGSLOPE

2309

Unsigned8

Read/Write

-